Unable to open drawing, failed to generate bookmark file

2021-10-06T23:27:21Z

Summary


Details

  ) In a test environment, user is unable to open drawing from Teamcenter to NX.
  ) Error of

    No bookmark file

    The server failed to generate the bookmark file.
    Please make sure that the dataset you intended to open is not a stand-alone dataset.

  ) User executed General... query to locate the drawing dataset,
    but double-click of the dataset results in the error.

  ) in Impact Analysis, Where Referenced indicates
    that the UGPART is *not* attached to an itemrevision.
    Hence, it is a standalone dataset.

  ) User located the model UGMASTER dataset and it *is* attached to an itemrevision.
  ) Also, Where Referenced on the UGMASTER showed that it is related to the UGPART.







Solution

  ) The drawing dataset had been accidentally cut from its itemrevision.
  ) User just had to paste the UGPART dataset to the itemrevision



Notes and References

  UGMASTER was related to the UGPART dataset with the relation = TC NX Master Model.



Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_OPEN

Ref: 002-8014106

KB Article ID# PL8014106

Contents

SummaryDetails

Associated Components