How to see if you have FloEFD HVAC module license inside Solid Edge?

2024-08-05T06:50:31Z

Summary


Details

The customer is running FloEFD for Solid Edge.

How to verify inside SE/FLoEFD whether HVAC (SE452F) is active?

Solution

There is no built-in check as to which license is checked out in FloEFD.  The easiest way is to check, is if the HVAC specific fields are there.  For example, look if 'Radiative Surface' is active under 'Conditions'

 


As 'radiative surface' is greyed out here, then the HVAC module is inactive.

Notes

If you have further inquiries about Solid Edge Solid Edge Portfolio Products Licensing please refer to the FAQs Collection link below:

Solid Edge Portfolio Products Licensing FAQs Collection


KB Article ID# PL8014084

Contents

SummaryDetails

Associated Components