Solid Edge How to control the "Custom Properties" within Solid Edge?

2021-10-06T23:55:40Z
PART/SHEETMETAL

Summary


Details

How to control the "Custom Properties" within Solid Edge? 

Solution

You can define registered custom properties in the propseed.txt file. The "propseed.txt" file is an ASCII text file that is used to populate values on the File Properties dialog box. To add values to the file, you can use a text editor, such as Notepad. This will allow you to customize lists for the following standard properties: title, category, keyword, and project name. 



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1709
Product: SOLID_EDGE
Application: SETUP
Version: V219.0
Function: INSTALL

Ref: 002-8014066

KB Article ID# PL8014066

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES