How to change the color of the Scale in a detail view caption?
Solution
The Drawing view caption is split into two components, "Primary caption" and "Secondary caption", and each component can have separate font formatting.
In this case, the Drawing View's name was placed in "Primary caption" and the scale was placed in "Secondary caption". The problem can be fixed in two ways: 1. The secondary caption's color can be changed to match the primary caption's color. or 2. The view scale string can be removed from the secondary caption and added to the primary caption itself.
You can predefine the caption text, colors and fonts for captions in the new Drawing View Style which is available in the style manager. You can also use Style mapping to setup specific styles for different drawing view types in the Solid Edge Options / Drawing View Style page.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: DRAFT
Version: V110MP12
Function: DRAWING_VIEWS
Ref: 001-9480691