How to export an assembly from NX to native with all part revisions?

2021-10-06T23:27:21Z

Summary


Details

How to export an assembly from NX to native with all part revisions?



Solution

Enable the customer default "Enable Multiple Revisions" in NX. 

From the NX Documentation:
https://docs.plm.automation.siemens.com/tdoc/nx/11.0.2/nx_help/#uid:tcin_multi_part_function 

If multiple revisions of a part exist in the original assembly, you can clone-export each part independently.


Here an example, how it works with ugmanager_clone functionality after customer default setting "Enable Multiple Revisions" was enabled:

In a Teamcenter command prompt change the path to NX installation:

%UGII_BASE_DIR%\UGMANAGER>Example for the ugmanager clone option whereAssembly is 00000040/A withcomponent: 00000004/A /B and actual RevCugmanager_clone -pim= -o=export -default_dir:"path for exported parts" -default_n=autotranslate -r="Working; Any Status" -asse=@DB\00000040\A -par=@DB\00000004\A -par=@DB\0000004\B

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: CLONE_EXPORT

Ref: 001-9472396

KB Article ID# PL8014018

Contents

SummaryDetails

Associated Components