Previously when selecting
Boundary Curves the
Member was always created as a
Tanto Tool Position. If the
Boundary Member needed to be switched to an
On Tool Position it would be done after it was selected. Can the
Tool Position type be set before the curve is selected?

Solution
Starting in
NX1847 there is a new option on the
Selection Bar when creating a
Planar Mill Boundary which allows the
Tool Position to be set before selecting the curve. This option is only available in a
Planar Mill operation.

Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1859
Function: BOUNDARIES
Ref: 002-8013985