Details
The Type Filter works not correctly.
If you choose a Feature Group under the function Extract Geometry to choose all solid Bodies inside, the solid and the sheet Body will Show.
When you choose with the same type filter, only the solid body will show.
Solution
It does not enforce current setting of Selection filter instead it takes over one of the allowed
entity types from the selection filter when the selected entity is not allowed by filter.
Selecting node from part Navigator will always collects bodies with Selection Intent(SI)
"Feature Bodies" rule irrespective of the rule set in SI toolbar.
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.1
Function: SELECT_INTENT
Ref: 002-8013963