When creating a dimension to point in scaled view, the value is incorrect. The value appears to be a scaled value (2x, 3x, etc) of the true value.
Solution
Determine that the point was actually created in the drafting view itself. To do so select the view and use MB3--> Expand. If you cannot see the point it likely resides on the drawing sheet.
To confirm, select the point and use MB3--> Properties--> Information icon and look for a line that reads "Resides on drawing" followed by the sheet name.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1847
Function: DIMENSION
Ref: 001-9467879