NX Save as the part with the same item type using Save As New Item Type command

2021-10-06T23:27:20Z
NX for Design

Summary


Details

Save as the part with the same item type using Save As New Item Type dialog

Solution

Save as the part with the same item type using Save As New Item Type dialog is blocked until user changes the item type to different item type, from NX12.0 onwards. 

If the user tries to save as the part keeping the same item type then he following warning is displayed.

====================================
Same Item Type
Same item type,use Save As New Item if type needs to be same
====================================


If user want to save as the part with the same item type, then use the command "Save As", change the Action to "New Item".

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_SAVE_AS

Ref: 002-8013926

KB Article ID# PL8013926

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX