NX Operations which result in Automatic check-out comments of UGMASTER
Solution
In NX, various automatic System generated comments are generated on various NX operations.
Below are the automatic check-out comments and their respective NX operations.
Set the TC preference "Check-out/Check-in Policy" to "Automatic Check-out on Modify or Save; Check-in on Save".
Modify the geometry and save as with the new item/revision.
Set the TC preference "Check-out/Check-in Policy" to "Automatic Check-out on Save; Check-in on Save"
Modify the geometry and then select "Check-out Modified Parts".
This will result into below Check-out comment.
Save one of the component in an assembly as Unique part.
This will result into below check-out comment.
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 764SP1
Product: NX
Application: NXMANAGER
Version: V11.0.2
Function: LOCKING
Ref: 002-8013925