Will Plant Simulation continue to support SimTalk version 1?

2021-10-07T00:01:46Z

Summary


Details

I have many old models that were made using SimTalk version 1. How long will Sim Talk 1 be supported?

Solution

Answer from development:

There are no plans to end support of SimTalk 1.


 Since it doesn't produce a big overhead to support it, there are also no reasons to stop support.


We have removed support of Syntax Indentation for SimTalk 1 in the latest version, but the methods will still run and you will be able to create new methods using SimTalk 1.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V15.0
Function: ALL

Ref: 002-8013903

KB Article ID# PL8013903

Contents

SummaryDetails

Associated Components