Solid Edge KeyShot 7 and 8 throw Open GL 2.0 error when using Remote Desktop

2021-10-06T23:55:37Z
APPLICATION

Summary


Details

Keyshot7 & 8 show an OpenGL 2.0 error when using Remote Desktop.



Solution

This is a limitation of running Remote Desktop. It is also reported in the actual KeyShot forums. 
The issue can also occur when running on a virtual machine, or any situation where graphics acceleration is not available. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 10_1803
Product: SOLID_EDGE
Application: APPLICATION
Version: V219MP6
Function: KEYSHOT

Ref: 001-9459376

KB Article ID# PL8013893

Contents

SummaryDetails

Associated Components

APPLICATION: KEYSHOT