Boundary selection in planar_mill (Tool_position)

2021-10-06T23:27:20Z

Summary


Details

Planar Mill operation - selecting boundaries. 
Boundary selection was improved at NX 11, but now it is not possible to directly select Tool Position 'ON' when selecting the boundary.



Solution

Select Tool Side = 'Right' or 'Left' and define the boundary 
In the Member 'List' , multiple select all of the members. (pick 'Member1' in the list, then hold the •Shift– key down and pick the last Member) 
Change Tool Position to 'On'



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: CAM
Version: V11.0
Function: PLANAR_MILLING

Ref: 001-9458808

KB Article ID# PL8013892

Contents

SummaryDetails

Associated Components