Simcenter 3D Solutions Why Browse function is not working in win 10 ?

2021-10-06T23:27:20Z
Simcenter 3D

Summary


Details

When browse a solution with windows7, the folder where the sim file exist in is opened.

 But when browse a solution with windows10, Microsoft Edge is started and nothing is displayed in Microsoft Edge.

 How to  make windows10 do the same behavior as windows7?

Solution

Folder is opening via *htm only.

User can change default browser as IE instead of Edge in Win 10.

 or if user want to keep only Edge as default browser ( NOT Interner Explorer) then you can change default application to open *htm document as IE.

Notes

KB Article ID# PL8013875

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow