Simcenter 3D Solutions How to use similar "Enforced motion location" of SC RD solution in SOL 103 ?

2021-10-06T23:27:20Z
Simcenter 3D

Summary


Details

How to use similar "Enforced motion location" of SC RD solution  in SOL 103 ?

Solution

"Enforced motion location" Boundary condition of  SC Response Dynamics solution will write SPC and USET card.

If the user  want to use the same in SOL 103, First create SPC and now create USET as per the steps below.

1.Edit the solution and switch to "bulk data"

2.Expand DOF sets

3.Now create a modelling object with the required Degrees of Freedom under USET,U2.

This is now equal to Enforced motion location of SC Response Dynamics solution 

Notes

KB Article ID# PL8013864

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow