How to change the ID field to Number in the NX File New dialog

2021-10-06T23:27:20Z

Summary


Details

How to change the 'ID' field on the NX File New dialog to 'Number' or 'ItemID' instead.



Solution

The 'ID' field on the NX File New dialog is being pulled from the Localization of the item_id property in BMIDE.
1. In BMIDE, Open the ItemType (that will be created on the NX File New dialog). 
    For example, open the ITEM ItemType.
2. Select the 'Properties' tab.
3. Highlight the 'item_id' property.
4. At the bottom, select the 'Localization' tab.
5. Highlight the 'ID' row, and select 'Override'.
6. In the Value Localization field, replace 'ID' with: Number
7. Finish the dialog.
8. Save and Deploy.
9. Now both Teamcenter and NX will use 'Number' instead of 'ID'.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1953
Function: FILE_NEW

Ref: 001-9457650

KB Article ID# PL8013851

Contents

SummaryDetails

Associated Components