PMI Callout in model does not show up in Draft?

2021-10-06T23:55:37Z

Summary


Details

PMI annotation/callouts in model do not show up in Draft view when retrieving dimensions/annotations. 



Solution

Even though the PMI callout did not have a leader which is not required, it still must be attached to some face, or edge of the model to appear in retrieve dimensions/annotations of draft. Once you do that and update the drawing view(s) it appears in the draft view. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219MP6
Function: PMI_MODEL_VIEW

Ref: 001-9455266

KB Article ID# PL8013825

Contents

SummaryDetails

Associated Components