Details
How to define multiple NX environments and select a specific environment from which to launch NX from Teamcenter?
Solution
This requires setting up NX environments in Teamcenter using the following preferences:
TC_NX_Environments
This is a multiple values preference containing a listing of the names of the NX environments.
Example:
NX11
NX12
NX1855
TC_NX_Location_for_ <one of the names of an NX environment from the above preference>
Example:
TC_NX_Location_for_NX11
TC_NX_Location_for_NX12
TC_NX_Location_for_NX1855
To select the desired NX environment to launch, use the User Settings dialog within Teamcenter to define it, hit to drop down for NX Environment to choose.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: TC_PORTAL
Ref: 002-8013793