Tecnomatix Unable to map .jt from Tecnomatix to Teamcenter

2021-10-07T00:01:38Z
eM-Server

Summary


Details

When trying to map ".jt" from Tecnomatix to Teamcenter as DirectModel dataset, getting a gear symbol (TMXMisc) instead of Directmodel dataset.



Solution

Do not create a new resource/part prototype in eMS and add the jt on the Attachments tab. Everything that shows up on the Attachments tab is automatically being mapped as TMXMisc, which is showing as a gear symbol in Teamcenter.


If the JT is added through the Physical tab (while standing on the prototype) then it should map correctly.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2008R2S1
Product: TECNOMATIX
Application: EM-SERVER
Version: V12.1.1.X
Function: CC

Ref: 001-7651205

KB Article ID# PL8013733

Contents

SummaryDetails

Associated Components

Collaboration Context Integration