PICK pose not attaching the part, only CLOSE pose works.

2021-10-07T00:01:36Z

Summary


Details

When using a Pick & Place operation, the pick pose "PICK" is not gripping the part. If the pick pose is changed to "CLOSE, the grip command works.



Solution

The issue is that the PICK pose did not allow the gripper tips to contact the part, so no attachment could be made. Changing the Offset value on the gripper definition allows attachment even if there was no contact between the gripper and the part. Issue is resolved.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 2012_R2
Product: TECNOMATIX
Application: ROBOTEXPERT
Version: V13.1
Function: ROBOTICS

Ref: 001-8954906

KB Article ID# PL8013727

Contents

SummaryDetails

Associated Components