Tecnomatix Option to turn off the Welcome Screen in 13.0.2

2021-10-07T00:01:33Z
eM-Server

Summary


Details

Need an option to turn off the Welcome screen, and for it to default back to the "Open Project" like past versions.



Solution

The Open Project style of startup is available if the "Enable Welcome Page" option is unchecked in the Tecnomatix Doctor Tools menu.


There is a CURRENT_USER registry entry to enable/disable the Welcome screen. 
The entry below shows the Welcome screen enabled. To make it disabled, modify the data value to zero. 


[HKEY_CURRENT_USER\Software\TECNOMATIX\TUNE\GeneralSettings\Options] 
"LandingPageEnabled"=dword:00000001



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: TECNOMATIX
Application: EM-SERVER
Version: V13.0.2
Function: ADMIN_TOOLS

Ref: 001-7906978

KB Article ID# PL8013721

Contents

SummaryDetails

Associated Components

eMS AdminConsole