How to create a reusable Logic Block for Process Simulate?

2021-10-07T00:01:33Z

Summary


Details

User has a logic block designed as a template that they wish to reuse in another study.


How to move it to a New Study?



Solution

A logic block is just a resource.

You can grab the cojt folder and insert it into another study just like any other component. It usually includes a jt file and a gmplc.xml file for the logic. 


You might need to delete the tunedata.xml and run "define component type" on it, but after that insert component will introduce it into any new study. 


The only thing missing will be the signals connected to the LB, which is study information, and must be reconnected manually or through the Connection Mapping tool.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V_UNKNOWN
Function: VIRT_COMMISSION

Ref: 001-8005426

KB Article ID# PL8013719

Contents

SummaryDetails

Associated Components