How to Customize the Default Files Name When Exporting a PDF.
Solution
Within NX select 'File -> Utilities -> Customer Defaults -> Gateway -> Plotting -> Job Name (tab) -> Entry 1, Entry 2 and Entry 3'.
The output file name has 3 separate entries to control it.
By default, the first called "Entry 1" is set to assign "the users login name", the second called "Entry 2" is set to assign "the part name", and the third called "Entry 3" is set to blank.
Therefore, by default, if you have a part file by the name "test.prt", then you will have a PDF file output name called "(your login name_test.pdf".
Users can change these setting in the Customer Defaults on this page.

Notes and References
This works for all releases of NX that can generate a PDF file.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 10_1703
Product: NX
Application: GATEWAY
Version: V1855
Function: PDF
Ref: 002-8013273