Clone assembly and be prompted to enter each component name

2019-06-06T19:31:18Z

Summary


Details

--------------- 
How can you clone an assembly and be prompted to enter each component name as 
well as the destination directory?



Solution

 1. Assemblies --> Cloning --> Create Clone Assembly.


2. Add Assembly button --> select assembly file (the cloning function works 
from the disk, not the NX session. You will be warned if the assembly in the 
session is the same as the assembly being cloned and the session version has 
been modified).


3. Execute button. You will be prompted to set the destination directory and 
name for each component starting with the assembly file (see the NX cue line 
for the current file to be renamed.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1876
Function: ASSEMBLY_MODEL

Ref: 001-6924865

KB Article ID# PL8011040

Contents

SummaryDetails

Associated Components