---------------
How can I set the XY Plotting tool to always plot in the Main Graphics Window?
Solution
To change the XY Plot options in NX 10, choose:
File-Preferences-XY Plot...
The XY Plot Preferences Window will pop up where users can set the Target
Graphic Window option. For this case, the user can select "Main Graphics
Window" and the plot will always be displayed in NX's Main Graphics window
without being prompted.
Other Target Window options are: "Separate Graphics Window" and "Both Windows
Allowed". The NX default is "Separate Graphics Window" and New Window;
"Always New Window".
Notes