Ribbon bar is disappearing and only the graphics window is displayed

2019-05-15T15:38:31Z

Summary


Details

Only the graphics window is displayed. The Ribbon is disappearing and missing.



Solution

This may be Full Screen mode.  If the mouse cursor is hovered over the thin grey strip at the top of the 
graphics window while in Full Screen mode, the ribbon bar will appear, and the 
button for Full Screen mode can be selected to toggle it off. 
Or, simply select Atl+Enter to exit Full Screen mode.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V10.0.3
Function: UI_TOOLS

Ref: 001-8949571

KB Article ID# PL8011035

Contents

SummaryDetails

Associated Components