What are 'Sticky Modules' and how do they work with bundles?

2019-08-21T12:16:22Z

Summary


Details

Sticky Modules were introduced as of NX 9.0 but there is not much information 
regarding them nor how they work.



Solution

Sticky Modules are special license features that allow NX to "create" bundles 
on the fly based on the user's usage of NX. They cost less than individual 
floating license features but have the caveat that they must be 'manually' 
released from a NX session. Sticky Modules will 'stick' to a bundle when they 
are checked out but won't be reserved when the bundle is initially accessed, 
unlike the components of a 'suite' bundle. A 'sticky module' will remain 
attached to the user's session until it is manually released via the NX 
utility 'Select Bundles' or by exiting out of NX.


For example, to manually release the Sticky License NX PMI / NXS10410 (i.e. 
MA_geometric_tol) from a NX session, do the following:


 File --> Start --> Gateway 
 File --> Utilities --> Select Bundles 
 Below "Licenses Attached To Bundle", select "MA_geometric_tol" 
 Then press the button "Free Selected Licenses" and press OK


The license is now available for the next user.



Notes and References

1. Sticky Modules only work for NX 9.0 and higher.


2. NX Product and Manufacturing Information (PMI) - S [NXS10410]


Description: 
NX Product and Manufacturing Information (PMI) - Sticky License NX PMI is an 
application that enables NX users to digitally author 3D annotation and 
product data in a solid part or assembly. PMI includes 3D dimensions, 3D GD&T 
(Geometric Dimension and Tolerance) data such as datums and feature control 
frames, 3D notes, and customizable non-geometric information that can be 
directly associated to an NX model. NX PMI is compliant with national and 
international 3D annotation standards. This module will remain attached to the 
user session until manually released.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V1872
Function: SYSTEM_TOOLS

Ref: 001-7572943

KB Article ID# PL8011030

Contents

SummaryDetails

Associated Components