Checking if components are fully constrained

2019-08-28T15:01:54Z

Summary


Details

--------------- 
How can you check if a component is fully constrained?



Solution

 To check if a component is fully constrained, select the component from the 
Assembly Navigator --> do a Right Mouse Button --> select "Show Degrees of 
Freedom". If the component is fully constrained it will not show any Degrees 
of Freedom and the Status line will read "There are no degrees of freedom".


Another option is to use Information --> Assemblies --> List Components. there 
will be a column for Positioned and it will list the components as Fully 
Constrained, Partially Constrainted, Fixed, or Absolute.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 864
Product: NX
Application: ASSEMBLIES
Version: V8.5
Function: POSITIONING

Ref: 001-7360759

KB Article ID# PL8011022

Contents

SummaryDetails

Associated Components