How to rotate an ISO view about drawing vertical axis

2019-06-06T15:40:00Z

Summary


Details

--------------- 
How to rotate the drawing ISO view about the vertical (Y axis) on the drawing sheet?



Solution

 To accomplish this the user needs to perform the following steps:


o Select the view boundary --> MB3 --> Edit 
o Select Model View --> Orient View Tool 
o Select the Z axis from the triad in the Orient View window 
o Enter 180 in the input field --> Enter --> OK



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1847
Function: DRAWING/VIEW

Ref: 001-7482440

KB Article ID# PL8011014

Contents

SummaryDetails

Associated Components