Secondary Tab is not possible to create after Three Bend Corner command is used

2019-10-30T14:49:33Z

Summary


Details

NX Sheet Metal - SB Three Bend Corner 
Treatment: Circular Cutout 
'Miter Corner' toggled ON (new at NX 9.0, default at NX 8.5 was OFF)) 
- This can then cause problems creating an SB Tab - which can fail with: 
'Error: Unable to create body'



Solution

Workaround: Toggle OFF 'Miter Corner'


This was fixed in NX 12.0  (ref PR 7323822)



Notes and References

7323822

Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: NX_SHEET_METAL
Version: V10.0.1
Function: CLOSED_CORNER

Ref: 001-7323822

KB Article ID# PL8011002

Contents

SummaryDetails

Associated Components