Collision Detection options are missing when moving a component

2019-05-15T17:27:56Z

Summary


Details

The 'Copy' and 'Collision Detection' groups are missing from the Move 
Component dialog.



Solution

 1. In the Assembly Navigator, highlight a component. 
2. MouseButton3-->Move. 
3. On the Move Component dialog, select the options button 
 in the dialog header. 
 NOTE: It looks like a gear in the upper left-hand corner. 
4. Select 'Move Component (More)'. 
 Now the 'Copy' and 'Settings' groups should appear in the dialog. 
5. Expand the 'Copy' group. 
6. Expand the 'Settings' group. 
7. Expand 'Collision Detection' to have access to the 
 Collision Detection options.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V8.5
Function: POSITIONING

Ref: 001-6989469

KB Article ID# PL8010992

Contents

SummaryDetails

Associated Components