Operations do not inherit values from the avoidance geometry parent.

2019-05-15T15:37:50Z

Summary


Details

A new operation placed under an avoidance parent does inherit those values.  If you manually change one of them by editing the operation itself, this overrides the inherited value.  Can you get this back or reverse the change?



Solution

Once you manually override an inherited avoidance parameter, that new value is used in the operation.  These are not handled in the same way as other inherited values, like tool information.  There is no lock/unlock icon to toggle between inherited or local values.  The avoidance parameters are pushed to the operation when it is created and from then on, any changes made at the operation level are what is used going forward.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: TURNING

Ref: 001-7786256

KB Article ID# PL8010978

Contents

SummaryDetails

Associated Components