How to transfer toolbar customizations to NX9

2019-05-15T15:37:46Z

Summary


Details


How to transfer toolbar customization's to NX9.



Solution

 In NX8.5, the 'user.mtx' file stores the toolbar customizations. It is located 
in the following directory: 
 C:\users\<username>\AppData\Local\Unigraphics Solutions\NX85


In NX9, the 'user.mtx' file is located in the following directory: 
 C:\Users\<username>\AppData\Local\Siemens\NX90


Copy the 'user.mtx' file from the NX8.5 location and paste it into the NX9 
location. The NX9 ribbon interface has changed from NX8.5 and it will transfer 
as many customizations as possible, but may not transfer them all.


Additionally in NX9 under 'Tools-->Customize' on the 'Roles' tab, there is an 
option, 'Add Custom Toolbars to Ribbon'. This option will create a custom 
ribbon tab. On the custom ribbon tab, all the unused user toolbars created 
interactively in Classic mode will be added as a group.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V9.0
Function: UI_TOOLS

Ref: 001-7325413

KB Article ID# PL8010975

Contents

SummaryDetails

Associated Components