How to place "2X" within Stacking bounding box.

2019-08-28T15:01:51Z

Summary


Details

--------------- 
When attempting to add a note to a stack of ID Symbols, the note does not get 
placed aligned to the ID Symbol.



Solution

 When adding the note, i.e "2X", go to Style and under the "Stacking" tab 
change the "Left/Right Alignment" from "Top" to "Middle", Select OK.


Then drag the Note to the ID Symbols so that the Stacking box appears and the 
"2X" will be placed next to the ID Symbol and aligned with the text in the ID 
Symbol.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V6.0
Function: FILE_NEW

Ref: 001-7110602

KB Article ID# PL8010974

Contents

SummaryDetails

Associated Components