NX Problem creating tool bit.

2019-09-04T13:01:37Z
NX for Manufacturing

Summary


Details

--------------- 
Needs to define holder with differnt fron insert orientation angle angle ?



Solution

 In the tool definition dialog you can choose an insert shape (from A 
Parallelogram 85 to X User defined) and you can combine it with a holder style 
(from A-Style to T-Style).


These combinations are fixed, the system orients the insert and the holder. 
If you change the inserts orient angle, the holder angle is changed by the 
same amount. If you change the holder angle, the inserts orient angle is also 
changed. As not all combinations of inserts and holders are captured by this, 
we introduced the new holder style "User Defined".


In this case, you can choose the orient angle for the insert and the holder 
angle separately. After an appropriate combination is found, you can toggle 
the "Lock Insert and Holder Orientation" button on. After the lock, changes of 
the inserts orient angle are also done for the holder angle, insert and holder 
are now fixed.


So, in short, the only way to define a holder and insert with different holder 
angle and insert orienttation angle is to use the'user-define' holder option.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: TURNING

Ref: 001-7756069

KB Article ID# PL8010969

Contents

SummaryDetails

Associated Components

Manufacturing General