A
Planar Mill operation is used to engrave logo geometry on a milling machine. How is this operation setup?

Solution
1. On the
Planar Mill dialog select the
Standard Drive Cut Pattern. Note that the menus seen below are from the new
Explorer menus. Though the menus are different the settings are the same as the legacy menus.

2. Add a Check mark to the
Cutting -> Strategy -> Self-Intersection option.

3. Uncheck the
Non Cutting -> More -> Collision Check option.

4. Before selecting curves or edges for
Part Boundaries set the
Tool Position On option from the
Selection Bar. This option causes the center of the tool to be kept on the curve instead of tangent to the curve. Also be certain to press
Add New Set after picking a set of connected curves. Selecting this option will cause a new boundary to be created. Creating multiple boundaries will cause a retract move to be included after cutting.

5. The operation might look something like the picture below when cutting.

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V1863
Function: PLANAR_MILLING
Ref: 001-7795331