NX After editing PAX files the Drawing Templates are not created as an assembly.

2019-08-28T15:01:43Z
NX for Design

Summary


Details

--------------- 
After editing the drawing pax file, the drawing templates that are used to 
create a master model drawing does not create a component beneath the drawing. 
The Assembly Navigator just shows a single node;


 123456-A-dwg1 of 123456


Should be:


 123456-A-dwg1 of 123456 
 | 
 123456



Solution

 The PAX file palette entry is missing the line for "UsesMasterModel"..


 <UsesMasterModel>Yes</UsesMasterModel>



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V7.5
Function: FILE_NEW

Ref: 001-7232114

KB Article ID# PL8010965

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX