Printing with the Autodesk DWF Writer (Freeware from Autodesk)

2019-08-12T13:25:37Z

Summary


Details

Is it possible to set up a PLOTTER to output drawings to an Autodesk DWF Writer?



Solution

 The Autodesk DWF writer is freeware from Autodesk;


http://usa.autodesk.com/dwf-writer/


The Autodesk DWF writer allows the user to create DWF files from many different applications. NX Plotting however, is not compatible with this software. The output formats that NX produces from Plotting are too complex for the DWF Writer to understand. 


However you can PRINT to the Autodesk DWF writer from NX by selecting 'File-> Print' from inside NX, once the Autodesk DWF writer software has been installed.


When Printing from NX, the Autodesk DWF Writer can be selected as a 'Printer'. Under Settings, select Black and White print.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: SYSTEM
Version: V1867
Function: WNT_OS_ISSUES

Ref: 001-7569931

KB Article ID# PL8010955

Contents

SummaryDetails

Associated Components