Simcenter 3D Solutions Incorrect Temperature profile for coupled cylinder to multi-layered shell

2019-05-16T19:02:16Z
Simcenter 3D

Summary


Details

--------------- 

When coupling cylindrical geometry modeled with multi-layered shells to a beam 

element that represents 1-D fluid flow, the thermal coupling connection 

performs a proximity check that picks out the closest elements. In curvilinear 

geometry, such as a cylinder that is meshed with a multilayer shell, this 

means that sometimes, the closest element is on the bottom layer. 

Unfortunately, the expectation is that the connection will connect to a 

different layer.

This situation is fairly common on the inside of airplanes. Users may have 

equipment which is hot and have rather small air flow rates passing over them. 

Users have been finding success using the 1-D fluid flow elements convecting to

solid surfaces. 

 

If there was the addition of a flag to override the proximity check, it would 

definitely be advantageous and prevent the users from changing models from 2-D 

shells to 3-D solids in order to arrive at correct solutions.

Solution

 In the latest TMG patch, nx10_tmg10.0.310_svn110163, an override flag is being 

introduced to override the proximity check.

The customer will need to create generic entity of type "INPF card". Then add 

the following information:

Card number: 9 

Text input: GPARAM 4 465 1

This will deactivate the proximity check.

Notes

KB Article ID# PL8010954

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow