Simcenter 3D Solutions Thermal Load with heater controller does not reach specified load

2020-08-28T22:39:15Z
Simcenter 3D

Summary


Details

--------------- 

I have a model with a heater controller connected to a thermal load. When 

looking at the applied load value, it does not match what I specified in the 

thermal load object. Why am I not seeing the full value I specified?

Solution

 There are three types of heater controllers available in NX Thermal/Flow: 

Proportional, PID controller, and Thermostat. The first two, Proportional and 

PID controller, scale the load based on how far the sensor element is away 

from the defined set point(s). They vary in how the scaling is defined, but 

they are both proportional type controllers. 

If the desire is to have a simple on/off for your load, then the user needs to 

select the third type, thermostat. With the thermostat heater controller when 

the temperature of the sensor element, or average temperature of the sensor 

elements, is below the cut-in temperature, the full load is applied. When the 

temperatuer of the sensor element reaches the cut-off temperature, then the 

load is turned fully off. 

For more details on these heater contollers see the following documents:

PID and Proportional heater controllers:

https://docs.plm.automation.siemens.com/tdoc/nx/10.0.3/nx_help/#uid:index_advan 

ced:xid389653:id1126083:id624386:id628376

Thermostat heater controller: 

https://docs.plm.automation.siemens.com/tdoc/nx/10.0.3/nx_help/#uid:index_advan 

ced:xid389653:id1126083:id624386:id628636

Notes

KB Article ID# PL8010950

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow