NX NX License Error when selecting 'Groove' and 'Slot' commands

2019-06-17T08:49:49Z
NX for Design

Summary


Details

The following NX error is displayed when either the 'Slot' or 'Groove' design feature commands are selected;


NX License Error: License server system does not support this feature [-18]


The cause of this error is that these commands require a "usr_defined_features" license, in NX 10.0, which may not be available in the license file.



Solution

This issue is resolved in the NX 10.0.1 maintenance release. 
The 'Groove' and 'Slot' commands can be accessed using a "features_modeling" license, as in previous versions of NX.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: DESIGN
Version: V10.0
Function: FEATURE_MODEL

Ref: 001-7314885

KB Article ID# PL8010949

Contents

SummaryDetails

Associated Components

Modeling