NX How to store settings in operation Display Options

2019-10-31T09:06:12Z
NX for Manufacturing

Summary


Details

How are operation 'Display Settings' stored in NX?



Solution

The settings are stored in each operation the way they were left - so if you edit an existing operation, it will have the settings that were last used in that operation 
 
For defaults in NEW operations being created , the settings are stored in each operation in the template parts 
 
for example , for a 'Floor & Wall' op , you would need to edit the mill_planar.prt (in MACH\resource\template_part\metric) 


- Then ( after restarting NX), when you create a new floor wall operation, you'll get those settings.


There is a customer default that specifies which template parts are used ( and so which ones you would need to edit) 



Manufacturing - General - 'Use Latest Updated Templates'


- If it is toggled OFF, then template parts under MACH\resource\template_part\metric are used 
- If it is toggled ON, then template parts under MACH\updates\template_part\metric are used 
 
(template parts under the 'updates' folder are sometimes updated when maintenance releases are installed - so these will change your settings back to the default)



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: NX
Application: CAM
Version: V10.0.3
Function: BASIC_FUNCTIONS

Ref: 001-8925291

KB Article ID# PL8010938

Contents

SummaryDetails

Associated Components

Manufacturing General