Remove Legacy Symbols Associated to Dimension Lines

2019-08-28T15:01:22Z

Summary


Details

--------------- 
Legacy Symbols Associated to Dimension Lines, gaps, finish symbols,etc.. how 
do you remove those symbols from the extension lines of a drafting dimension in 
NX10 & NX11?



Solution

 Prior to NX10, the Component tool from the Edit pulldown was available to use 
to remove the symbols from the drafting objects.


If the Component tool is not available, you will need to add to a menu or to 
the ribbon bar.


Go to;


 - Tools --> Customize 
 - expand Menu 
 - select Edit 
 - drag "Component..." to a menu or ribbon bar. 
 - close Customize. 
 
To delete the symbols do the following;


 - Select the Component tool that you added, 
 - toggled ON the "Delete Component" option, 
 - select the Drafting object,i.e. the dimension. 
 - select the symbol component. 
 - Apply.


The symbol will be removed from the dimension.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: XP64_SP2
Product: NX
Application: DRAFTING
Version: V10.0
Function: SYMBOL

Ref: 001-8902352

KB Article ID# PL8010937

Contents

SummaryDetails

Associated Components