Drive the position of a section line using a dimension

2019-05-15T15:37:25Z

Summary


Details

How to drive a Drawing section line's position using a dimension.



Solution

 NX allows the creation of a sketch curve to position the Section Line and then 
create a driving dimension to re-position the Section Line as needed.


1. In the Part Navigator, hover the cursor over the Parent view (of the 
 Section view to be created), 'MouseButton3 (MB3)-->Active Sketch 
 View'. 
 Note: Direct Sketch curves can now be added associatively to the 
 Parent view. 
2. Insert a Sketch line segment (Vertical or Horizontal) in the Parent 
 view where the initial cut location of the Section line will be. 
3. Select the 'Finish' icon to finish the sketch. 
4. Select the 'Section View' icon. 
5. For the Cut position, select the control point of the sketch curve 
 from Step 3 and create the Section Line. 
6. Place the Section View. 
7. Select the 'Linear Dimension' icon. 
 NOTE: Confirm the 'Driving Method' is set to 'Driving'. 
8. Select the Sketch curve from Step 3 for the first object. 
 Select the second object and place the dimension. 
 Note: The Section Line is now associated to the sketch curve and 
 can be moved if the dimension is modified.


To modify the dimension that moves the Section Line: 
1. Double-click the dimension to edit it. 
2. On the Dimension dialog, enter a new value to move the sketch curve. 
4. Update the drawing, and the Section View will update.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V9.0
Function: DRAWING/VIEW

Ref: 001-8803467

KB Article ID# PL8010935

Contents

SummaryDetails

Associated Components