How to edit the Mirror Part Type in a linked mirrored part

2019-05-15T15:37:22Z

Summary


Details

In a linked mirrored part, how can the 'Mirror Part Type' be edited from 'Exact 
Mirror' to 'Non-exact Mirror - Keep Broken Links'?



Solution

 The main difference between 'Exact Mirror' and 'Non-exact Mirror - Keep Broken 
Links' is as follows:


Exact Mirror = when the source entities are deleted, the mirrored part 
 will immediately delete the resulting broken linked features. 
Non-exact Mirror - Keep Broken Links = when the source entities are deleted, 
 the mirrored part will contain broken linked features which 
 will not be deleted.


If an 'Exact Mirror' part needs to be changed to a 'Non-exact Mirror - Keep 
Broken Links' part, this can be done by editing the MirrorPartType attribute. 
1. Open the 'Exact Mirror' part. 
2. In the Assembly Navigator, select the part. 
3. MouseButton3-->Properties. 
4. In the Properties dialog, select the 'Attributes' tab. 
5. Select the attribute: MirrorPartType 
6. The Value drop-down will have 3 values. 
 - ExactMirror 
 - NonExactMirrorKeepLinks 
 - NonExactMirrorDeleteLinks 
7. Toggle the Value drop-down to: NonExactMirrorKeepLinks 
8. OK the Displayed Part Properties dialog. 
9. Select 'File-->Save' to save the part after this change. 
This will internally update the MirrorPartType attribute for this particular 
mirror part. The mirror part update behavior will be according to the 
MirrorPartType attribute value chosen.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V8.5
Function: WAVE

Ref: 001-7267413

KB Article ID# PL8010930

Contents

SummaryDetails

Associated Components