Radius to Center dimension style

2019-06-06T17:21:17Z

Summary


Details

--------------- 
How can you create a radial dimension with a leader that extends to the center 
of the radius?



Solution

 To get the Radius to Center dimension style like prior to NX9, you have to use the Radial dimension icon on the ribbon toolbar --> set the method to Radial --> select the circle/arc to dimension in the graphics window --> MB3 -> you should see Radius to Center.


Note: If you use the Rapid dimension, you can access Radial dimension but you won't get the Radius to Center option.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V1876
Function: DIMENSION

Ref: 001-7737375

KB Article ID# PL8010923

Contents

SummaryDetails

Associated Components