NX How can an existing view be Oriented using the Orient View Tool?

2019-08-28T15:01:03Z
NX for Design

Summary


Details

--------------- 
User added a 3D Shaded View to the drawing. Now the user wants to change 
the orientation of the part using the View Orient Tool window that was used 
when the view was added to the drawing. Where is the View Orient Tool?



Solution

 Select the drawing view from the Part Navigator or from the view boundary, use 
the Right Mouse Button and select Edit. In the Model View section of the Base 
View dialog the Orient View Tool is available.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: DRAFTING
Version: V8.5
Function: DRAWING/VIEW

Ref: 001-7737346

KB Article ID# PL8010911

Contents

SummaryDetails

Associated Components

Drafting