---------------
How to add tool parameters to the posted file for review by the machine
operator.
Solution
Import the custom command pb_cmd_tool_list.tcl to your postprocessor.
- Open your postprocessor
- Select the Program & Tool Path tab and then select the Custom Command tab (please see image below.


Select pb_cmd_tool_list.tcl and select Open from the "Explorer" dialog box.
Follow the instructions detailed in PB_CMD_create_tool_list.
Notes and References
Alternate Solution:
When postprocessing, turn on the review tool. A good resource is the doc below..
https://docs.plm.automation.siemens.com/tdoc/nx/1847/nx_help/#uid:xid916262Tip:To search for an event or variable, you can use a text editor to search for it in the output file that is named in the title bar of the NX/Post Review Tool dialog box. The file is located in the same location as the post output, and has the name format <login_name><several digits>_review.out . To find a variable that corresponds to a parameter, a good tip is to type a unique value in the corresponding operation dialog box, for example 12345.6789, 9999.9999, or a few digits of pi (3.14159), or anything that you can search for without getting too many results. Search for it in the *_debug.outfile. Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: CAM
Version: P1859
Function: POSTBUILDER
Ref: 001-7349547