NX In order to save a CGM, the sheet must be displayed at the time of save.

2019-05-08T07:04:16Z
NX for Design

Summary


Details

--------------- 
During part file save in the Modeling Application the following message is 
shown:


Save CGM 
Parts containing sheets that are not visible will not have a CGM saved with them and existing CGM's will be deleted. 
In order to save a CGM the sheet must be displayed at the time of save. 
Do you want to continue?


A similar message is shown when exporting a file to CGM or PDF:


Parts containing sheets that are not visible will not have a CGM / PDF exported.
In order to export a CGM / PDF the sheet must be displayed at the time of export.



Solution

 The message indicates that when saving a part file the CGM data for the drawing sheets will not be saved if these are not displayed. 
When f.i. in the Modeling Application the drawing sheets are not displayed. 
When saving the part file in the Modeling Application the drawing CGM will not be saved in the NX part. If any drawing CGM was stored in the part, it will be deleted. 
When saving the part in the Drafting Application the CGM data will be saved in the part file.


Outside the Drafting Application the drawing status is not visible. The sheets can be out-of-date. The design has been changed in NX 11.0 to prevent out-of-date sheets to be saved or exported. In the Drafting Application it is still possible to save or export out-of-date drawing sheets. However, in the Drafting 
Application the drawing status is visible, so the user is aware of the out-of-date status.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: GATEWAY
Version: V11.0
Function: CGM_EXPORT

Ref: 001-8330883

KB Article ID# PL8010907

Contents

SummaryDetails

Associated Components

Modeling