NX Cannot Use Numeric Keypad to Set Places to Right of Decimal

2023-08-21T10:28:42Z
NX Open NX for Manufacturing Licensing Teamcenter Share NX System Administration NX Design Translators NX for Design

Summary


Details

Cannot Use Numeric Keypad to Set Places to Right of Decimal.

Solution

Pre-NX10 releases users in Drafting could press a keypad number to alter the number of decimal places which was removed in NX10 and later releases.

In NX10 and later releases users must press the "Alt and Numeric Keypad Number" at the same time and with the number lock turned on and active to achieve this result.This will change the number of places to the right of the decimal or comma in adimension dynamically.

Note that the keypad does not work at all in NX9.

Legacy behavior: NX8.5 and earlier only required users to press the keypad values with the number lock turned on and active.

Notes

KB Article ID# PL8010905

Contents

SummaryDetails

Associated Components

Block/UI Interface Stylers Knowledge Fusion Menuscript NX Open - All Languages NX Open Python Open for C/C++ Open for CAE Open for GRIP Open for Java Pre-NX6 UI Styler SNAP UDO